| Solid Edge Part Type Library : SimplifiedAssemblyModel Object |
AddMeasureVariable | Returns the measure variable object. |
BindKeyToObject | Binds a specified reference key to a specified Occurrence, SubOccurrence, or TopologyReference object. |
BreakAllInterpartLinks | |
FreezeAllInterpartLinks | |
GetBaseStyle | Returns the base style. |
GetInContextAssemblyNameForInterpartLinks | |
GetRayIntersections | Returns intersection points, normal at points, intersection types and intersection information for a set of bodies and set of rays |
GoalSeek | |
HasInterpartLinks | |
ImportStyles | Imports the styles from the document given by Filename into the referenced document. If Overwrite is true, any duplicate styles will be overwritten. |
MeasureAngle | Measures the sharp angle between lines or planes or keypoints. |
MinimumDistance | Measures the minimum distance between two elements. |
NormalDistance | Measures the normal distance between lines or planes. |
PMI_ByModelState | Get PMI dimensions and annotations by model state. Returns failure for invalid states. |
QueryByEntity | |
QueryByProperty | Returns a SEGenericCollection object that consists of AttachedProperty objects that match all of the query inputs. |
Redo | Reapplies actions reversed via Undo. |
SetBaseStyle | Returns the base style. |
ShowParentsAndChildren | |
ThawAllInterpartLinks | |
ToggleRefPlanesDisplay | Controls the display of the reference planes. |
Undo | Reversed a specified number of actions. |
BodyCheck | Specifies whether or not the referenced document object contains a valid parasolid body. |
Constructions | Returns the Constructions collection object. |
CoordinateSystems | Represents a collection of CoordinateSystem objects. |
DesignBodyVisible | Specifies whether or not the referenced object is displayed to the screen. |
DesignEdgebarFeatures | |
DimensionStyles | |
FaceStyles | Returns the FaceStyles collection object for the referenced document. |
FillStyles | Returns the FillStyles collection object for the referenced document. |
GeometricVersion | Returns a value that is incremented each time the geometry of an associated document is changed. |
HatchPatternStyles | Returns the HatchPatternStyles collection object for the referenced document. |
HoleDataCollection | Returns the HoleDataCollection object for the referenced document object. |
InterpartLinks | |
LinearStyles | Returns the LinearStyles collection object for the referenced document. |
Models | Returns the Models collection object for the referenced document object. |
ProfileSets | Returns the ProfileSets collection object for the referenced document object. |
RefAxes | Returns the RefAxes collection object for the referenced document object. |
RefPlanes | Returns the RefPlanes collection object for the referenced document object. |
ShowCurvatureCombs | Toggles the display of curvature combs for the referenced object. |
Sketches | Returns the Sketches collection object for the referenced document object. |
Variables | Returns the Variables collection object for the referenced document. |
ViewStyles | Returns the ViewStyles collection object for the referenced document. |