Solid Edge Part Type Library
MinimumDistance Method
Description
Measures the minimum distance between two elements.
Syntax
Visual Basic
Public Sub MinimumDistance( _
   ByVal Element1 As Object, _
   ByVal Element2 As Object, _
   ByRef Distance As Double, _
   ByRef Point1() As Double, _
   ByRef Point2() As Double _
) 
Parameters
Element1
Element2
Distance
Point1
Point2
See Also

SimplifiedAssemblyModel Object  | SimplifiedAssemblyModel Members

Send comments on this topic.