Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
EnableRegions | Specifies whether or not the Sketch will display regions. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsUnderDefined | This read-only Boolean property returns True when the referenced ProfileSet object is underdefined (that is, insufficiently constrained geometrically). |
Locked | Specifies whether or not the Sketch is locked as the active sketch. |
MergeWithCoplanarSketches | Specifies whether or not the Sketch merges with co-planar sketches. |
MigrateGeometryAndDimensions | Specifies whether the sketch geometry will be migrated and moved to a used sketch when used to create a feature. |
MirrorPlane | This read-write property sets and returns the plane about which to mirror for the referenced object. |
MirrorSketch | This read-write property sets and returns the mirror sketch for the referenced Sketch object. |
ModelingModeType | Returns the modeling mode of the referenced object. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
Profile | Returns the Sketch's Profile object. |
Profiles | Returns the Profiles collection object. |
ShowSketchColors | Specifies whether the sketch colors or the element colors are displayed for the referenced object. |
Status | Returns the status of the specified object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
Type | Specifies the type of the object being referenced. |