Solid Edge Part Type Library
Profiles Property
Description
Returns the Profiles collection object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Profiles As Profiles
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objSketch As SolidEdgePart.Sketch
    Dim objProfiles As SolidEdgePart.Profiles
    Dim objProfile As SolidEdgePart.Profile
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a Sketch object
    Set objSketch = objDoc.Sketches.Add
    Set objProfiles = objSketch.Profiles
    Set objProfile = objProfiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
    Call objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)

    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSketch = Nothing
    Set objProfile = Nothing
    Set objProfiles = Nothing
End Sub
See Also

Sketch Object  | Sketch Members

Send comments on this topic.