Solid Edge Part Type Library
DraftFromOutsideEdges Property
Description
Specifies how draft angle is measured for the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property DraftFromOutsideEdges As Boolean
Remarks
When set to True, the draft angle is measured from the faces that are closest to the sketch that defines the feature. When set to False, the draft angle is measured from the faces that are farthest from the sketch that defines the feature.
See Also

Vent Object  | Vent Members

Send comments on this topic.