|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  DraftAngle | Specifies the draft angle. | 
|  DraftEnabled | Specifies whether draft is enabled. | 
|  DraftFromOutsideEdges | Specifies how draft angle is measured for the referenced object. | 
|  DraftSide | Specifies the draft side. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  ExtentDepth | Sets and returns the extent depth. | 
|  ExtentSide | Sets and returns the extent side. | 
|  ExtentType | Sets and returns the extent type. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  ModelingModeType | Returns the modeling mode of the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  RibDepth | Specifies the rib depth. | 
|  RibExtension | Specifies the distance the ribs extend past the exterior boundary. | 
|  RibOffset | Specifies the distance the ribs are offset from the entrance surface. | 
|  RibThickness | Specifies the rib thickness. | 
|  RoundEnabled | Specifies whether rounding is enabled for the referenced object. | 
|  RoundRadius | Specifies the round radius. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  SparDepth | Specifies the spar depth. | 
|  SparExtension | Specifies the distance the spars extend past the exterior boundary. | 
|  SparOffset | Specifies the distance the spars are offset from the entrance surface. | 
|  SparThickness | Specifies the spar thickness. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |