Solid Edge Part Type Library
DraftSide Property
Collapse All
Expand All
Solid Edge Part Type Library
>
Vent Object
: DraftSide Property
Description
Specifies the draft side.
Property type
Read-write property
Syntax
Visual Basic
Public Property DraftSide As
VentDraftSideConstants
Remarks
Sets and returns the side of the draft plane to which the draft angle is applied relative to the zero degree direction. The draft side controls whether the draft is inward or outward.
See Also
Vent Object
|
Vent Members
Send comments
on this topic.