| StructureEditor Namespace : IStructureEditor Object |
GetBOMViewSetInCombo | |
GetDisplayAlerts | This API is used to get the status of display alerts property whether it is ON or OFF. |
Quit | This API is used to quit the structure editor application. |
SetBOMViewInCombo | |
SetDisplayAlerts | This API is used to set the display alerts property ON or OFF. If this property is ON then certain alerts and messages will be displayed while the application is running. If this property is OFF then the operation will be performed silently without any alerts and messages. |