Imports System.IO
Imports System.Runtime.InteropServices
Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As StructureEditor.Application = Nothing
        Dim objStructureEditor As StructureEditor.SEECStructureEditor = Nothing
        Dim bDisplayAlerts As Boolean = False
        Try
            OleMessageFilter.Register()
            ' Start structure editor application
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("StructureEditor.Application"))
            objStructureEditor = objApplication.SEECStructureEditor
            objApplication.Visible = True
            objApplication.GetDisplayAlerts(bDisplayAlerts)
            If bDisplayAlerts Then
                ' Alerts and messages will be displayed while the application is running.
            Else
                ' Alerts and messages will not be displayed while the application is running.
            End If
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            If Not objApplication Is Nothing Then
                ' Kill the instance of structure editor created
                objApplication.Quit()
            End If
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module