| StructureEditor Namespace : SEECStructureEditor Object |
AddExistingItem | This API is used to add the given Item into specified item. |
AddItemInMultipleFiles | |
AddItemToGivenProjects | This API is used to add the Item to given projects. |
AddNewItem | This API is used to add the new empty item into specified item. |
AssignAll | This API is used to automatically assign system generated values to the mandatory properties of a document like item id,item revision,item name and dataset name. |
ClearAllActions | This API is used to clear the action, if any set on the solid edge file. |
Close | This API is used to close the solid edge file. |
CreateRootNewItem | This API is used to create root new empty item. |
GetProjectsForGivenItemID | This API is used to get the projects for GivenItemID. |
GetProjectsForLoggedInUser | This API is used to get the projects for logged in User. |
Open | This API is used to open a solid edge file from the teamcenter server into structure editor. |
PerformActions | This API is used to perform actions set on the solid edge file. |
RemoveItem | This API is used to remove the given Item from specified item. |
SetReplaceSelected | This API is used to replace the existing item with new item. |
SetReviseAll | This API is used to set revise action on all open solid edge files in structure editor. |
SetReviseSelected | This API is used to set revise action on a selected file in the structure editor. |
SetSaveAsAll | This API is used to set save as action on all the open files in the structure editor. |
SetSaveAsSelected | This API is used to set save as action on a selected solid edge file in the structure editor. |
SetSaveAsSpecificOccurrence | |
ValidateLogin | This API is used to login to teamcenter server. |