StructureEditor Namespace
PerformActions Method
Description
This API is used to perform actions set on the solid edge file.
Syntax
Visual Basic
Public Function PerformActions() As Long
Remarks
Call this API after setting action on the solid edge file. Do not forget to assign values after setting the action. If the values are not set on the mandatory parameters of the solid edge file then the action will not be performed.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As StructureEditor.Application = Nothing
        Dim objStructureEditor As StructureEditor.SEECStructureEditor = Nothing
        Dim strItemId As String
        Dim strItemRev As String
        Dim strFileName As String
        Dim strRevisionRule As String
        Dim strFolderName As String

        Try
            OleMessageFilter.Register()

            ' Start structure editor application
            objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("StructureEditor.Application"))
            objStructureEditor = objApplication.SEECStructureEditor
            objApplication.Visible = True

            strItemId = "081691"
            strItemRev = "A"
            strFileName = "a.asm"
            strRevisionRule = "Latest Working"
            strFolderName = ""

            If objStructureEditor.Open(strItemId, strItemRev, strFileName, strRevisionRule, strFolderName) = 0 Then
                If objStructureEditor.SetReviseSelected(strItemId, strItemRev, strFileName = 0) Then
                    If objStructureEditor.AssignAll() = 0 Then
                        objStructureEditor.PerformActions()
                    End If
                End If
            End If
        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            If Not objApplication Is Nothing Then
                ' Kill the instance of structure editor created
                objApplication.Quit()
            End If

            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

SEECStructureEditor Object  | SEECStructureEditor Members

Send comments on this topic.