Solid Edge ST7 SDK
Solid Edge ST2 MP1 - What's New
Problem Reports
Item Description
PR 2130405 Problems occur when "Addin" is registered in "Quick Access Toolbar"
PR 1566510 OpenSave macro fails with runtime error if file has status 'in work'
PR 1729888 third party add-in added to QAT works first time but if SE is closed and re-opened
PR 2130772 CommandBarButton::BeginGroup Property has no effect
PR 2129831 In SynchronousParts, "CopySurface.Type Property" cannot be acquired
PR 2129884 Implemented InterpartConstructions and InterpartConstruction automation methods
PR 1751696 SEPreview causes application termination
New APIs
None
See Also