Solid Edge ST7 SDK
Solid Edge ST3 MP11 - What's New
Problem Reports
Item Description
PR 1860707 Tube creation was dramatically slowed-down in ST4 due to material update.
PR 6587188 User requests new event be fired
PR 6570990 Fixed an abort at HReGenerateSlot
PR 6590564 Fixed a problem saving 3D-PDFs via automation
PR 6562523 center-plane relationship automation support
PR 6574228 API access to Assembly variables in broken in ST4
PR 1853189 It is not possible to set/get occurrence visibility in edit mode via API
PR 6585353 BalloonDisplayedText API does not return the correct info.
PR 1861355 Product Aborts when loading a customization file with "deny" security
PR 1844579 Need Automation support for creating PMI dimensions
PR 1852602 Replace part which belongs to a part family doesn't invoke OnFileOpenUI
PR 6578131 Added automation method to get associated assembly occurrence from draft
PR 1860716 Writing properties and dynamic attributes is very slow in ST4 after placing part
New APIs
None
See Also