Solid Edge Assembly Type Library
IsAttributeSetPresent Property
Description
Returns True if a specified Attribute Set exists on the referenced object.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsAttributeSetPresent( _
   ByVal Name As String _
) As Boolean
Parameters
Name
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objAxialRel As SolidEdgeAssembly.AxialRelation3d
    Dim objAttributeSets As Object
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    Dim bAttribSetPresent As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a particular axial relation in the collection
    Set objAxialRel = objDoc.Relations3d.Item(2)
    ' Get the AttributeSets collection object
    Set objAttributeSets = objAxialRel.AttributeSets
    'Create an AttributeSet
    objAttributeSets.Add "MyAttribSet"
    'Check for the presence of the AttributeSet
    bAttribSetPresent = objAxialRel.IsAttributeSetPresent("MyAttribSet")
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objAxialRel = Nothing
    Set objAttributeSets = Nothing
End Sub
See Also

AxialRelation3d Object  | AxialRelation3d Members