Solid Edge Assembly Type Library
AxialRelation3d Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method FlipChecks the current orientation of the referenced object and sets it to its opposite value.
Public Method GetElement1Returns the first element in this relationship.
Public Method GetElement2Returns the second element in this relationship.
Public Method GetGeometry1Returns the geometry of the referenced object.
Public Method GetGeometry2Returns the geometry of the referenced object.
Public Method SelectSelects the referenced object in the active window.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DetailedStatusReturns the detailed status of the Relation3d object.
Public Property FixedParallelOffsetSpecifies whether or not a fixed parallel offset is to be applied to the relationship.
Public Property FixedRotateSpecifies whether or not the rotation is to be fixed for the referenced AxialRelation3d object.
Public Property IndexReturns the numeric index for the active object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property Occurrence1Returns the first Occurrence object for the referenced relationship object.
Public Property Occurrence2Returns the second Occurrence object for the referenced relationship object.
Public Property OffsetSets or returns the distance that two parts are offset from one another.
Public Property OrientationSets and returns the axial orientation state.
Public Property ParallelOffsetSpecifies whether parallel offset is applied to the relationship.
Public Property ParentReturns the parent object for the referenced object.
Public Property RangedOffset
Public Property RangeHigh
Public Property RangeLow
Public Property StatusReturns the status (a member of the Relation3dStatusConstants constant set) of the referenced Part.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property TypeA member of the ObjectType constant set.
See Also

AxialRelation3d Object