Solid Edge Assembly Type Library
Suppress Property
Description
Temporarily suppresses the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Suppress As Boolean
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objAxialRel As SolidEdgeAssembly.AxialRelation3d
    ' Local variables to be declared here
    Dim bSuppress As Boolean
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
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
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Open an existing assembly document
    Set objDoc = objApp.Documents.Open(TESTFILE)
    'Get a particular AxialRelation from the collection
    Set objAxialRel = objDoc.Relations3d.Item(2)
    'Get the Suppress state of the AxialRelation
    bSuppress = objAxialRel.Suppress
    'Change the Suppress state
    objAxialRel.Suppress = Not bSuppress
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objAxialRel = Nothing
End Sub
See Also

AxialRelation3d Object  | AxialRelation3d Members