Solid Edge Assembly Type Library
GetOrigin Method
Returns the x coordinate of the Occurrence's point of origin.
Returns the y coordinate of the Occurrence's point of origin.
Returns the z coordinate of the Occurrence's point of origin.
Description
Returns the origin for the referenced object.
Syntax
Visual Basic
Public Sub GetOrigin( _
   ByRef OriginX As Double, _
   ByRef OriginY As Double, _
   ByRef OriginZ As Double _
) 
Parameters
OriginX
Returns the x coordinate of the Occurrence's point of origin.
OriginY
Returns the y coordinate of the Occurrence's point of origin.
OriginZ
Returns the z coordinate of the Occurrence's point of origin.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPart As SolidEdgeAssembly.Occurrence
    Dim dblOriginX As Double
    Dim dblOriginY As Double
    Dim dblOriginZ As Double
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    Call objDoc.Close
    ' opening an existing assembly file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' getting a part in the assembly
    Set objPart = objDoc.Occurrences.Item(3)
    ' getting the origin of the placed part
    Call objPart.GetOrigin(OriginX:=dblOriginX, OriginY:=dblOriginY, OriginZ:=dblOriginZ)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPart = Nothing
End Sub
See Also

Occurrence Object  | Occurrence Members