Solid Edge Assembly Type Library
IsNongraphic Property
Collapse All
Expand All
Solid Edge Assembly Type Library
>
Occurrence Object
: IsNongraphic Property
Description
Returns True if the referenced Occurrence is non-graphic, false if it is not.
Property type
Read-only property
Syntax
Visual Basic
Public Property IsNongraphic As Boolean
Remarks
Returns True if the Occurrence is non-graphic, false if it is not.
See Also
Occurrence Object
|
Occurrence Members