Solid Edge Assembly Type Library
PutOrigin Method
Specifies the x coordinate of the new origin.
Specifies the y coordinate of the new origin.
Specifies the z coordinate of the new origin.
Description
Sets a new origin for the referenced object.
Syntax
Visual Basic
Public Sub PutOrigin( _
   ByVal OriginX As Double, _
   ByVal OriginY As Double, _
   ByVal OriginZ As Double _
) 
Parameters
OriginX
Specifies the x coordinate of the new origin.
OriginY
Specifies the y coordinate of the new origin.
OriginZ
Specifies the z coordinate of the new origin.
Remarks
The coordinates are defined from the model base coordinate system.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPart As SolidEdgeAssembly.Occurrence
    Dim dblOriginX As Double
    Dim dblOriginY As Double
    Dim dblOriginZ As Double
    Const TESTFILE = "T:\vbtests\testcases\cube.par"
    ' Report errors
    Const PI = 3.14159265358979
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' adding a part document to the assembly document
    Set objPart = objDoc.Occurrences.AddByFilename(OccurrenceFileName:=TESTFILE)
    ' changing the origin of the placed part
    dblOriginX = 0.05
    dblOriginY = 0.025
    dblOriginZ = 0.075
    Call objPart.PutOrigin(OriginX:=dblOriginX, OriginY:=dblOriginY, OriginZ:=dblOriginZ)
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPart = Nothing
End Sub
See Also

Occurrence Object  | Occurrence Members