Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgeAssembly.AssemblyDocument
Dim objPart As SolidEdgeAssembly.Occurrence
Dim dblAxisX1 As Double
Dim dblAxisX2 As Double
Dim dblAxisY1 As Double
Dim dblAxisY2 As Double
Dim dblAxisZ1 As Double
Dim dblAxisZ2 As Double
Const TESTFILE = "T:\vbtests\testcases\cube.par"
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' adding a part document to an assembly document
Set objPart = objDoc.Occurrences.AddByFilename(OccurrenceFileName:=TESTFILE)
' rotating the placed part in the assembly
dblAxisX1 = 0
dblAxisX2 = 0.01
dblAxisY1 = 0
dblAxisY2 = 0.01
dblAxisZ1 = 0
dblAxisZ2 = 0.01
Call objPart.Rotate(AxisX1:=dblAxisX1, AxisY1:=dblAxisY1, AxisZ1:=dblAxisZ1, _
AxisX2:=dblAxisX2, AxisY2:=dblAxisY2, AxisZ2:=dblAxisZ2, Angle:=PI / 3)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objPart = Nothing
End Sub