| Solid Edge Assembly Type Library : PhysicalProperties Object |
GetAsmPhysicalPropsRelativeToCoordSystem | Returns the results of the last physical property calculations performed on the assembly relative to a coordinate system. |
GetAssemblyPhysicalProperties | Returns the results of the last physical property calculations performed on the assembly. |
GetAssemblyPhysicalProperties1 | |
GetSelectSetPhysicalProperties | Returns the physical property calculations for the active select set. |
GetSelectSetPhysicalPropsRelativeToCoordSystem | Returns the physical property calculations for the active selection set relative to a coordinate system. |
SetUserDefinedAssemblyPhysicalProperties | Set user defined physical properties to the physical property object of an assembly. |
Update | Updates the referenced object. |
WriteToFile | Creates a text file that contains the physical property information for the referenced assembly. |
Application | Returns the active application object. |
DisplayCenterOfMass | Controls the display in the assembly of the center-of-mass graphics. |
DisplayCenterOfVolume | Controls the display in the assebmly of the center-of-volume graphics. |
DisplayPrincipalAxes | Controls the display in the assembly of the principal axes graphics. |
IsUpToDate | Returns and sets the status of the assembly's physical properties. |
Parent | Returns the parent object for the referenced object. |
UpdateOnFileSaveStatus | Check or uncheck "Update on File Save" check box. |
UserDefinedPropertiesStatus | Check or uncheck "User-defined properties" check box. |