Solid Edge Assembly Type Library
DisplayCenterOfMass Property
Description
Controls the display in the assembly of the center-of-mass graphics.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayCenterOfMass As Boolean
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objPhyProps As SolidEdgeAssembly.PhysicalProperties
    Const TESTFILE = "T:\vbtests\testcases\Sample.asm"
    Dim bMass As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Close the active document
    Call objDoc.Close
    ' opening an existing assembly file
    Set objDoc = objApp.Documents.Open(TESTFILE)
    ' Getting the PhysicalProperties object of the assembly document
    Set objPhyProps = objDoc.PhysicalProperties
    ' Getting DisplayCenterOfMass property of PhysicalProperties object
    bMass = objPhyProps.DisplayCenterOfMass
    objPhyProps.DisplayCenterOfMass = Not bMass
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objPhyProps = Nothing
End Sub
See Also

PhysicalProperties Object  | PhysicalProperties Members