Solid Edge Assembly Type Library
TangentRelation3d Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GetElement1Returns the first element in this relationship.
Public Method GetElement2Returns the second element in this relationship.
Public Method GetGeometry1Returns the geometry of the referenced object.
Public Method GetGeometry2Returns the geometry of the referenced object.
Public Method SelectSelects the referenced object in the active window.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property DetailedStatusReturns the detailed status of the Relation3d object.
Public Property HalfSpacePositiveIndicates whether the referenced TangentRelation3d is placed on the positive normal side of a plane (True) or the reverse normal side of a plane (False).
Public Property IndexReturns the numeric index for the active object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property Occurrence1Returns the first Occurrence object for the referenced relationship object.
Public Property Occurrence2Returns the second Occurrence object for the referenced relationship object.
Public Property OffsetSets or returns the distance (in working units) that two parts are offset from one another.
Public Property ParentReturns the parent object for the referenced object.
Public Property RangedOffset
Public Property RangeHigh
Public Property RangeLow
Public Property StatusReturns the status of the specified object.
Public Property SuppressTemporarily suppresses the referenced object.
Public Property TypeSpecifies the type of the object being referenced.
See Also

TangentRelation3d Object