Solid Edge Assembly Type Library
Index Property
Description
Returns the numeric index for the active object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Index As Long
Remarks
This index is the sequence that the object holds in its collection object (as held by the parent).
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeAssembly.AssemblyDocument
    Dim objTangntRelation As SolidEdgeAssembly.TangentRelation3d
    ' Local variables to be declared here
    Const TESTFILE = "T:\vbtests\testcases\TangntRel3d.asm"
    Dim lngIndex As Long
    ' Create/get the application with specific settings
    On Error Resume Next
    Set objApp = GetObject(, "SolidEdge.Application")
    If Err Then
        Err.Clear
        Set objApp = CreateObject("SolidEdge.Application")
        Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    objDoc.Close False
    'Open an existing Assembly containing TangentRelation
    Set objDoc = objApp.Documents.Open(Filename:=TESTFILE)
    'Get hold of the TangentRelation from the Relations3d collection
    Set objTangntRelation = objDoc.Relations3d(2)
    'Get the Index of the TangentRelation
    lngIndex = objTangntRelation.Index
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objTangntRelation = Nothing
End Sub
See Also

TangentRelation3d Object  | TangentRelation3d Members