Solid Edge Assembly Type Library
InsideArea Property
Collapse All
Expand All
Solid Edge Assembly Type Library
>
Tube Object
: InsideArea Property
Description
Returns the area in square meters (expressed as a Double) of the inside area of the referenced Tube object.
Property type
Read-only property
Syntax
Visual Basic
Public Property InsideArea As Double
Remarks
If the tube is solid, the InsideArea property returns 0.
See Also
Tube Object
|
Tube Members