Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
DefaultBendRadius | Sets and returns the default bend radius for the referenced Tube object. |
ExtentEnd | Specifies the tube extent end. |
ExtentStart | Specifies the tube extent start. |
InsideArea | Returns the area in square meters (expressed as a Double) of the inside area of the referenced Tube object. |
InsideVolume | Returns the volume in cubic meters (expressed as a Double) of the inside volume of the referenced Tube object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
IsSolid | Returns True if the referenced object encloses a finite, well-defined, volume. |
Material | Sets and returns the material (expressed as an existing FaceStyle object) of the referenced Tube object. |
MinimumFlatLength | Sets and returns the minimum allowable length of a straight tube for the referenced Tube object. |
OuterDiameter | Sets and returns the outer diameter of the referenced Tube object. |
Parent | Returns the parent object for the referenced object. |
PartFileName | Returns the fully qualified path name of the Part file associated with the referenced Tube object. |
TubeMaterial | Sets and returns the material (expressed as an existing FaceStyle object) of the referenced Tube object. |
UsesGlobalBendRadius | Specifies whether or not the referenced Tube object uses the global bend radius for the associated AssemblyDocument. |
UsesGlobalMinimumFlatLength | Specifies whether or not the referenced Tube object uses the global minimum flat length for the associated AssemblyDocument. |
UsesGlobalOuterDiameter | Specifies whether or not the referenced Tube object uses the global outer diameter for the associated AssemblyDocument. |
UsesGlobalWallThickness | Specifies whether or not the referenced Tube object uses the wall thickness for the associated AssemblyDocument. |
WallThickness | Specifies a wall thickness to be applied to the referenced Tube object. |