Solid Edge Assembly Type Library
InsideVolume Property
Description
Returns the volume in cubic meters (expressed as a Double) of the inside volume of the referenced Tube object.
Property type
Read-only property
Syntax
Visual Basic
Public Property InsideVolume As Double
Remarks
If the tube is solid, the InsideVolume property returns 0.
See Also

Tube Object  | Tube Members