Solid Edge Assembly Type Library
IsSolid Property
Description
Returns True if the referenced object encloses a finite, well-defined, volume.
Property type
Read-write property
Syntax
Visual Basic
Public Property IsSolid As Boolean
Remarks
This does not necessarily imply that each Face, for example, is connected at all its edges. The Body may still consist of standalone Faces that collectively define a finite volume.
See Also

Tube Object  | Tube Members