Solid Edge Assembly Type Library
Material Property
Collapse All
Expand All
Solid Edge Assembly Type Library
>
Tube Object
: Material Property
Description
Sets and returns the material (expressed as an existing FaceStyle object) of the referenced Tube object.
Property type
Read-write property
Syntax
Visual Basic
Public Property Material As
FaceStyle
Remarks
The default value is Copper.
See Also
Tube Object
|
Tube Members