Solid Edge Draft Type Library
DraftDocument Object Members
Overview 
Public Methods
Public Method ActivateMakes the referenced object the active one.
Public Method AnnotationTrackerStatisticsReturns the number of Annotations, Hole Tables and Parts Lists that are changed or detached during drawing view update
Public Method ClearAllDimensionTrackerEntriesClears all dimension tracker entries.
Public Method CloseCloses the referenced object.
Public Method CreatePreview
Public Method DimensionTrackerEntry
Public Method DimensionTrackerNumEntries
Public Method DimensionTrackerStatisticsReturns the number of dimensions that are changed or detached during drawing view update
Public Method DimensionTrackerStatisticsExReturns the number of dimensions and annotations that are changed or detached or rebound during drawing view update
Public Method EditPropertiesDisplays the EditProperties dialog box to allow the user to interactively set and view various properties of the referenced document object.
Public Method GetGlobalParameterReturns the setting of a specified global parameter for the referenced Application or document object.
Public Method GetObjectFromKeyReturns the object associated with the specified key.
Public Method GetSymbolFileOriginGets the origin used when the draft file is placed as a embedded or linked symbol. This function will fail if no origin has been defined.
Public Method GoalSeek
Public Method ImportStyles2Copies styles of the specified type from the specified document. If bReplace is False, only styles that do not already exist will be copied.
Public Method NewWindowCreates a new window that contains the referenced document.
Public Method PopulateQuicksheetTemplatePopulates the existing Quicksheet template drawing views with the model specified.
Public Method PrintOutPrints the contents of the referenced object.
Public Method PrintOutExPrints the contents of the referenced object.
Public Method SaveSaves the referenced object.
Public Method SaveAsSaves the referenced document to a new name, directory, or format.
Public Method SaveAsJTSaves the referenced document to JT format with specified options.
Public Method SaveCopyAsSaves a copy of the referenced document to a file without modifying the open document.
Public Method SeekReadOnlyAccess
Public Method SeekWriteAccessSeeks write access to the document if it is available.
Public Method SendMailDistributes the referenced document using the installed electronic mail system.
Public Method SetFilenameForDVWizardSets the file name to be used by the Drawing View wizard. The Drawing View wizard will clear this value.
Public Method SetGlobalParameterSets the value of a specified global parameter for the referenced Application or document object.
Public Method SetSymbolFileOriginSets the origin used when the draft file is placed as a embedded or linked symbol.
Public Method UpdatePropertyTextCacheAndDisplayUpdate the property text cache and Refresh the display
Public Method UpdatePropertyTextDisplayRefresh the display of the property text
Public Properties
Public Property ActivePrintingSheetReturns the Sheet object currently being printed.
Public Property ActiveSectionReturns the active sheet's Section object. Sheets are grouped into sections: WorkingSection, BackgroundSection, and 2dModelSection.
Public Property ActiveSectionTypeSpecifies the type of Section that the active sheet is a member of.
Public Property ActiveSheetReturns the active Sheet object.
Public Property ActiveSketchReturns the active Sketch object.
Public Property AddInsStorageReturns an IUnknown pointer to the object that implements the IStorage corresponding to the add-in substorage for the referenced object.
Public Property ApplicationReturns the active application object.
Public Property AttributeQueryReturns the AttributeQuery object.
Public Property BlocksReturns the collection of blocks in the document.
Public Property BlockTableEventsContains the AfterUpdate event.
Public Property BlockTablesReturns the associated BlockTables object for the referenced DraftDocument object.
Public Property ConnectorTableEventsContains the AfterUpdate event.
Public Property ConnectorTablesReturns the associated ConnectorTables object for the referenced DraftDocument object.
Public Property CreatedVersionReturns the version of Solid Edge that was used to create the referenced document.
Public Property DashStylesThis read-only property returns the DashStyles collection object for the referenced DraftDocument object.
Public Property DimensionStylesReturns the DimensionStyles collection object for the referenced document.
Public Property DirtySpecifies whether or not the referenced document has been modified since the last time it was saved.
Public Property DisplayAlignmentIndicatorSets and returns whether or not the alignment indicator is displayed.
Public Property DisplayRelationshipHandlesSets and returns whether or not relationship handles are displayed.
Public Property DocumentEventsReturns the DocumentEvents object for the referenced document object.
Public Property DraftBendTableEventsContains the AfterUpdate event.
Public Property DraftBendTablesReturns the associated DraftBendTables object for the referenced DraftDocument object.
Public Property DrawingViewEventsReturns the DrawingViewEvents object for the referenced DraftDocument object.
Public Property DrawingViewStylesReturns the DrawingViewStyles collection object for the referenced document.
Public Property FeatureControlFrameDataSetsReturns the FeatureControlFrameDataSets collection object for the referenced document.
Public Property FilePreferencesGet and set file level preferences.
Public Property FillStylesReturns the FillStyles collection object for the referenced document.
Public Property FullNameReturns the name and path of the referenced object.
Public Property HatchPatternStylesReturns the HatchPatternStyles collection object for the referenced document.
Public Property HighlightSetsReturns the HighlightSets collection object for the referenced document object.
Public Property HoleTablesReturns the HoleTables collection object.
Public Property InactiveDrawingViewModeSets and returns the inactive drawing view mode on the document.
Public Property InPlaceActivatedSpecifies whether or not the referenced document is in-place activated.
Public Property IsInsightFileReturns indication of whether the file is an Insight managed file.
Public Property IsTemplateSpecifies whether or not the referenced document is a template.
Public Property LastSavedVersionReturns the version of Solid Edge that was used the last time the referenced document was saved.
Public Property LinearStylesReturns the LinearStyles collection object for the referenced document.
Public Property MaintainRelationshipsReturns whether maintain relationships is enabled or disabled
Public Property ModelLinksReturns the ModelLinks collection object for the referenced document.
Public Property NameReturns the name of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PartsListEventsContains the AfterUpdate event.
Public Property PartsListsReturns the associated PartsLists object for the referenced DraftDocument object.
Public Property PathReturns the directory path name of the referenced document.
Public Property PropertiesFor document objects, returns the PropertiesCollection colletion object. For Variables, sets and returns the variable properties.
Public Property QuicksheetTemplateCountReturns the count of Quicksheet drawing views.
Public Property ReadOnlySpecifies whether or not the referenced document has been opened as read-only.
Public Property RootStorageReturns the IUnknown pointer to the object implementing the root storage of the referenced document.
Public Property RoutingSlipReturns the RoutingSlip object for the referenced document.
Public Property SectionsReturns the Sections collection object for the referenced document. Sheets are grouped into sections: WorkingSection, BackgroundSection, and 2dModelSection.
Public Property SelectSetReturns the current selection set for the referenced document.
Public Property SheetGroupsReturns a collection of working sheet groups.
Public Property SheetsReturns a collection of sheets that belong to the referenced object.
Public Property SmartFrame2dStylesReturns the SmartFrames2d collection object for the referenced document.
Public Property StatusReturns the status of the specified object.
Public Property SummaryInfoReturns a SheetSummaryInfo object to provide access to descriptive properties for the referenced document.
Public Property SurfaceFinishSymbolDataSetsReturns the SurfaceFinishSymbolDataSets collection object for the referenced document.
Public Property SymbolPropertiesReturns the SymbolProperties collection object for the referenced document.
Public Property TablesReturns the collection of user tables in the document.
Public Property TableStylesReturns the TableStyles collection.
Public Property TextCharStylesReturns the TextCharStyles collection object for the referenced document.
Public Property TextStylesReturns the TextStyles collection object for the referenced document.
Public Property TypeSpecifies the type of the object being referenced.
Public Property UndoStepsThis read-write Long property sets and returns the number of undo steps for the referenced document object.
Public Property UnitsOfMeasureReturns the UnitsOfMeasure object for the referenced document.
Public Property VariablesReturns the Variables collection object for the referenced document.
Public Property WeldSymbolDataSetsReturns the WeldSymbolDataSets collection object for the referenced document.
Public Property WindowsReturns the Windows collection object.
See Also

DraftDocument Object