Private Sub btnImportStyles_Click(sender As System.Object, e As System.EventArgs) Handles btnImportStyles.Click
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
Dim objDoc2 As SolidEdgeDraft.DraftDocument
Dim objType As Type = Nothing
Try
objApplication = GetObject(, "SolidEdge.Application")
If objApplication Is Nothing Then
' Get the type from the Solid Edge ProgID
objType = Type.GetTypeFromProgID("SolidEdge.Application")
' Start Solid Edge
objApplication = Activator.CreateInstance(objType)
' Make Solid Edge visible
objApplication.Visible = True
End If
objDraftDoc = objApplication.ActiveDocument
objDoc2 = objApplication.Documents.Open("C:\Program Files (x86)\Solid Edge ST6\Training\stddb3d.dft")
Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igDimensionStyle, False, objDoc2)
Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igLineStyle, False, objDoc2)
Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igTableStyle, True, objDoc2)
Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igFillStyle, True, objDoc2)
Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igHatchStyle, True, objDoc2)
Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igDrawingViewStyle, True, objDoc2)
Call objDraftDoc.ImportStyles2(SolidEdgeFramework.seStyleTypeConstants.igTextStyle, True, objDoc2)
Catch ex As Exception
MsgBox(ex.ToString)
End Try
End Sub