Solid Edge FrameworkSupport Type Library
Arcs2d Collection Members
Overview 
Public Methods
Public Method AddAsFilletCreates an Arc2d object that connects to two intersecting graphics objects.
Public Method AddAsFilletNoTrimCreates an Arc2d object that connects to two intersecting graphics objects.
Public Method AddByCenterStartEndCreates an Arc2d object by three points: the center point, the start point, and the end point.
Public Method AddByStartAlongEndCreates an Arc2d object by three points: the start point, a point along the arc, and the end point.
Public Method ItemThe items in a collection.
Public Properties
Public Property ApplicationReturns the active application object.
Public Property CountReturns the number of objects in the referenced collection.
Public Property ParentReturns the parent object for the referenced object.
See Also

Arcs2d Collection