Solid Edge FrameworkSupport Type Library
BalloonSides Property
Description
Sets and returns the number of sides for an N-sided balloon.
Property type
Read-write property
Syntax
Visual Basic
Public Property BalloonSides As Integer
Remarks
This property only pertains to N-sided Balloon objects. All sides of the balloon are equal and tangent to a circle whose diameter is defined by the BalloonSize property. Also, the shape is always drawn such that one side is horizontal, and this side is located at the bottom edge of the circle.
See Also

Balloon Object  | Balloon Members