Solid Edge FrameworkSupport Type Library
BalloonSize Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
Balloon Object
: BalloonSize Property
Description
Sets and returns the size of the referenced Balloon object.
Property type
Read-write property
Syntax
Visual Basic
Public Property BalloonSize As Double
Remarks
The default size is 12mm. The balloon's size must be greater than 0 and cannot be null.
See Also
Balloon Object
|
Balloon Members