Solid Edge FrameworkSupport Type Library
BreakLineDistance Property
Description
Sets and returns the length along the x axis that the break line traverses.
Property type
Read-write property
Syntax
Visual Basic
Public Property BreakLineDistance As Double
Remarks
This property is only enabled if the BreakLine property is True.
See Also

Balloon Object  | Balloon Members