Solid Edge FrameworkSupport Type Library
GetAlignmentShape Method
Description
Returns alignment shape and alignment shape point
Syntax
Visual Basic
Public Sub GetAlignmentShape( _
   ByRef AlignmentShapeObj As Object, _
   ByRef x As Double, _
   ByRef y As Double _
) 
Parameters
AlignmentShapeObj
x
y
Example
Imports System.Runtime.InteropServices
Public Class Balloon_GetSetAlignmentShape

    Private Sub btnGetSetAlignmentShape_Click(sender As System.Object, e As System.EventArgs) Handles btnGetSetAlignmentShape.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objLine As SolidEdgeFrameworkSupport.Line2d = Nothing
        Dim objCircle As SolidEdgeFrameworkSupport.Circle2d = Nothing
        Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objAlignmentShape As SolidEdgeFrameworkSupport.AnnotAlignmentShape = Nothing
        Dim objType As Type = Nothing
        Dim DrawingView As SolidEdgeDraft.DrawingView = Nothing
        Dim DrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim DrawingView1 As SolidEdgeDraft.DrawingView = Nothing
        Dim balloons As SolidEdgeFrameworkSupport.Balloons = Nothing
        Dim balloon As SolidEdgeFrameworkSupport.Balloon = Nothing
        Dim itemNumberDir As SolidEdgeFrameworkSupport.DimItemNumDirConstants = Nothing
        Dim objFirstballoon As SolidEdgeFrameworkSupport.Balloon = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objAnnotAlignmentShapes As SolidEdgeFrameworkSupport.AnnotAlignmentShapes = Nothing
        Dim objAnnotAlignmentShape As SolidEdgeFrameworkSupport.AnnotAlignmentShape = Nothing
        Dim dPointX(0 To 5) As Double
        Dim dPointY(0 To 5) As Double
        Dim dPointX1(0 To 5) As Double
        Dim dPointY1(0 To 5) As Double
        Dim dPointX2(0 To 5) As Double
        Dim dPointY2(0 To 5) As Double

        Dim PointX As Double
        Dim PointY As Double

        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If
            'Get reference to active document
            objDraftDoc = objApplication.ActiveDocument
            'Get reference to sheet
            objSheet = objDraftDoc.ActiveSheet

            'Populate array for x-coordinate of points of Annotation Alignment Shape
            dPointX(0) = 0.0
            dPointX(1) = 0.1
            dPointX(2) = 0.1
            dPointX(3) = 0.0
            dPointX(4) = 0.0
            'Populate array for y-coordinate of points of Annotation Alignment Shape
            dPointY(0) = 0.0
            dPointY(1) = 0.0
            dPointY(2) = 0.1
            dPointY(3) = 0.1
            dPointY(4) = 0.0

            objAnnotAlignmentShapes = objSheet.AnnotAlignmentShapes
            'Add balloon in the sheet
            balloons = objSheet.Balloons
            balloon = balloons.Add(0.1, 0.1, 0)
            balloon.Leader = True
            balloon.AddVertex(0.1, 0.1, 0)

            ' for AddAnnotAlignmentShape and other properties specific to alignment shapes.
            objAnnotAlignmentShape = objAnnotAlignmentShapes.AddAnnotAlignmentShape(dPointX, dPointY)

            Call balloon.SetAlignmentShape(objAnnotAlignmentShape, 0.05, 0.0)
            Call balloon.GetAlignmentShape(objAlignmentShape, PointX, PointY)
        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub

End Class
See Also

Balloon Object  | Balloon Members