Solid Edge FrameworkSupport Type Library
DimensionScale Property
Description
Sets and returns the scale factor of the referenced object.
Property type
Read-write property
Syntax
Visual Basic
Public Property DimensionScale As Double
Remarks
If the ScaleMode is manual, this value is used to scale the dimension value. The dimension scale is an inverse property; that is, a dimension scale of 0.5 doubles the dimension.
See Also

DimStyle Object  | DimStyle Members