Solid Edge FrameworkSupport Type Library
OffsetLeaderType Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimStyle Object
: OffsetLeaderType Property
Description
Sets and returns the type of offset leader to be drawn.
Property type
Read-write property
Syntax
Visual Basic
Public Property OffsetLeaderType As
DimOffsetLeaderTypeConstants
Remarks
The Offset Leader Line is valid only when the text is offset.
See Also
DimStyle Object
|
DimStyle Members