Solid Edge FrameworkSupport Type Library
TerminatorInsideLimit Property
Description
Toggles the associated dimension to the outside of the projection when the dimension value is less than the terminator inside limit.
Property type
Read-write property
Syntax
Visual Basic
Public Property TerminatorInsideLimit As Double
Remarks
When the dimension value is less than the value of the TerminatorInsideLimit property (specified as a ratio of text height), the associated dimension is automatically positioned outside of the projection.
See Also

DimStyle Object  | DimStyle Members