Solid Edge FrameworkSupport Type Library
VerticalLimitsGap Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimStyle Object
: VerticalLimitsGap Property
Description
Sets and returns the vertical limits gap between the limit value texts.
Property type
Read-write property
Syntax
Visual Basic
Public Property VerticalLimitsGap As Double
Remarks
The value is ratio to text.
See Also
DimStyle Object
|
DimStyle Members