Solid Edge FrameworkSupport Type Library
VerticalToleranceGap Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
DimStyle Object
: VerticalToleranceGap Property
Description
Sets and returns the vertical tolerance gap between the dimension value and the tolerance text.
Property type
Read-write property
Syntax
Visual Basic
Public Property VerticalToleranceGap As Double
Remarks
The value is ratio to text.
See Also
DimStyle Object
|
DimStyle Members