Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfile As SolidEdgePart.Profile
Dim objD1 As SolidEdgeFrameworkSupport.Dimension
Dim objA1 As SolidEdgeFrameworkSupport.Arc2d
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Create an empty Profile
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1))
' Create an Arc
Set objA1 = objProfile.Arcs2d.AddByCenterStartEnd(xCenter:=0, yCenter:=0, _
xStart:=0, yStart:=0.01, xEnd:=0.01, yEnd:=0)
' Creating a Dimension object
Set objD1 = objProfile.Dimensions.AddAngle(Object:=objA1)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfile = Nothing
Set objD1 = Nothing
Set objA1 = Nothing
End Sub