Private Sub Form_Load()
Dim objApp As SolidEdgeFramework.Application
Dim objDoc As SolidEdgePart.PartDocument
Dim objProfile As SolidEdgePart.Profile
Dim objC1 As SolidEdgeFrameworkSupport.Circle2d
Dim objD1 As SolidEdgeFrameworkSupport.Dimension
Dim sDumpStatus As String ' Used for temporary storage of datadump return string
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Create a Profile
Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
objDoc.RefPlanes(1))
' Create a Circle object in the Profile
Set objC1 = objProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.01)
' Create a Dimension object
Set objD1 = objProfile.Dimensions.AddRadius(Object:=objC1)
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
Set objProfile = Nothing
Set objC1 = Nothing
Set objD1 = Nothing
End Sub