Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objDimns As SolidEdgeFrameworkSupport.Dimensions
    Dim objApplicn As SolidEdgeFramework.Application
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create a Circular Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(objDoc.RefPlanes(1))
    ' Creating a Dimensions Collection object
    Set objDimns = objProfile.Dimensions
    ' Get the Application Property
    Set objApplicn = objDimns.Application
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objDimns = Nothing
    Set objApplicn = Nothing
End Sub
See Also

Dimensions Collection  | Dimensions Members