Solid Edge FrameworkSupport Type Library
AxisMode Property
Description
Sets and returns the axis mode from which the Dimension measurement axis is found.
Property type
Read-write property
Syntax
Visual Basic
Public Property AxisMode As DimAxisModeConstants
Remarks
Valid values are members of the DimAxisModeConstants constant set.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objProfile As SolidEdgePart.Profile
    Dim objDimns As SolidEdgeFrameworkSupport.Dimensions
    Dim cDimAxisMode As DimAxisModeConstants
    Dim sDumpStatus As String    ' Used for temporary storage of datadump return string
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' Create an empty Profile
    Set objProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:= _
                                                         objDoc.RefPlanes(1))
    Set objDimns = objProfile.Dimensions
    'Set the Axis Mode
    objDimns.AxisMode = igDimAxisModeDefault
    ' Get the Axis Mode
    cDimAxisMode = objDimns.AxisMode
    ' USER DISPLAY
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objProfile = Nothing
    Set objDimns = Nothing
End Sub
See Also

Dimensions Collection  | Dimensions Members