Solid Edge FrameworkSupport Type Library
Application Property
Description
Returns the active application object.
Property type
Read-only property
Syntax
Visual Basic
Public Property Application As Application
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame
    Dim objFCFApp As SolidEdgeFramework.Application
    ' Local variables to be declared here
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Add a new FeatureControlFrame
    Set objFCF = objFCFs.Add(x:=0.1, y:=0.1, z:=0)
    objFCF.PrimaryFrame = "FLVB0.001MCVBA"
    'Get the Application object from FeatureControlFrame
    Set objFCFApp = objFCF.Application
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
    Set objFCF = Nothing
    Set objFCFApp = Nothing
End Sub
See Also

FeatureControlFrame Object  | FeatureControlFrame Members