Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
BoxAlignment | Sets and returns the status of the alignment of a feature control frame.
Note: This is a multi-level feature control option. if it's set true value, all first and second box would align and text move to the center of box. |
BreakLine | Specifies whether or not a breakline is added between the leader line and the referenced dimensioning object. |
BreakLineDirection | Sets and returns the direction (left or right) in which the break line runs along the x axis. |
BreakLineDistance | Sets and returns the length along the x axis that the break line traverses. |
CompositePrimaryAndSecondaryText | Sets and returns the composite status of primary and secondary text. |
CompositeSecondaryAndTertiaryText | Sets and returns the composite status of secondary and tertiary text. |
CompositeTertiaryAndQuaternaryText | Sets and returns the composite status of tertiary and quaternary text. |
Document | Returns the document to which the referenced object belongs. |
FCFAllAround | Specifies whether or not an all around symbol is to be applied to the Leader of the referenced object. |
FCFAllOver | Specifies whether or not an all over symbol is to be applied to the Leader of the referenced object. |
FCFBorderPointCount | Returns the number of border points on the object. |
HidePMI | Show or Hide the referenced PMI Feature Control Frame object. |
Index | Returns the numeric index for the active object. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Key | Returns a key (a string) to find the object relative to its owning parents. |
KeyPointCount | Returns the number of keypoints/handles that are supported by the referenced object. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Leader | Specifies whether or not the referenced object has a leader line. |
LeaderTextConnectionPoint | Sets and returns the connection point of FCF text with leader or breakline. |
Name | Returns the name of the referenced object. |
Orientation | Sets and returns the orientation of feature control frame. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
PMIName | Get and set the name of reference PMI annotation object. |
PMIPlane | |
PMITrackDistance | |
PrimaryFrame | Sets and returns the primary frame text. |
QuaternaryFrame | Sets and returns the quaternary frame text. |
RotationAngle | Sets and returns the angle, in radians, at which the object is rotated along its major axis. |
SecondaryFrame | Sets and returns the secondary frame text for the referenced FeatureControlFrame object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
TertiaryFrame | Sets and returns the tertiary frame text. |
TextScale | Sets and returns the text scale of the object. |
Type | Specifies the type of the object being referenced. |
VertexCount | Returns the number of vertices in the referenced object. |
ZOrder | Specifies the front-to-back order in which an object is displayed relative to other objects. |