Solid Edge FrameworkSupport Type Library
GetTerminator Method
Specifies the object to which the terminal end of a dimensioning or annotation object's leader connects.
Coordinates of the leader's terminal connect point on the TerminatorObj.
Coordinates of the leader's terminal connect point on the TerminatorObj.
Coordinates of the leader's terminal connect point on the TerminatorObj.
Returns True if the leader was placed with respect to the TerminatorObj. Returns False if the leader was placed with respect to a key point on the TerminatorObj.
Description
Returns the object to which the terminal end of a dimensioning or annotation object's leader connects.
Syntax
Visual Basic
Public Sub GetTerminator( _
   ByRef TerminatorObj As Object, _
   ByRef x As Double, _
   ByRef y As Double, _
   ByRef z As Double, _
   ByRef keyPoint As Boolean _
) 
Parameters
TerminatorObj
Specifies the object to which the terminal end of a dimensioning or annotation object's leader connects.
x
Coordinates of the leader's terminal connect point on the TerminatorObj.
y
Coordinates of the leader's terminal connect point on the TerminatorObj.
z
Coordinates of the leader's terminal connect point on the TerminatorObj.
keyPoint
Returns True if the leader was placed with respect to the TerminatorObj. Returns False if the leader was placed with respect to a key point on the TerminatorObj.
Remarks
This method also returns the coordinates of the leader's terminal connect point and a Boolean value to indicate whether the leader was placed with respect to the object or with respect to a key point on that object.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objLine As SolidEdgeFrameworkSupport.Line2d
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame
    Dim objTerminator As SolidEdgeFrameworkSupport.Line2d
    ' Local variables to be declared here
    Dim dblX As Double, dblY As Double, dblZ As Double
    Dim bKeyPoint As Boolean
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Draw a line to be set as terminator object for the FeatureControlFrame
    Set objLine = objSheet.Lines2d.AddBy2Points(x1:=0.1, y1:=0.1, x2:=0.2, y2:=0.1)
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Add a new FeatureControlFrame
    Set objFCF = objFCFs.AddByTerminator(TerminatorObject:=objLine, x:=0.125, y:=0.1, z:=0, Keypoint:=False)
    objFCF.PrimaryFrame = "FLVB0.001MCVBA"
    Call objFCF.AddVertex(x:=0.2, y:=0.2, z:=0)
    objFCF.BreakLine = True
    Call objFCF.GetTerminator(terminatorobj:=objTerminator, x:=dblX, y:=dblY, z:=dblZ, _
                              Keypoint:=bKeyPoint)
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objLine = Nothing
    Set objFCFs = Nothing
    Set objFCF = Nothing
    Set objTerminator = Nothing
End Sub
See Also

FeatureControlFrame Object  | FeatureControlFrame Members