Solid Edge FrameworkSupport Type Library
GetVertices Method
Returns the number of vertices in the vertex array.
Returns an array of vertices.
Description
Returns an array of vertex coordinates in a dimensioning object.
Syntax
Visual Basic
Public Sub GetVertices( _
   ByRef VertexCount As Long, _
   ByRef Vertices() As Double _
) 
Parameters
VertexCount
Returns the number of vertices in the vertex array.
Vertices
Returns an array of vertices.
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame
    ' Local variables to be declared here
    Dim dblVertices() As Double
    Dim lngVertexCount As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Add a new FeatureControlFrame
    Set objFCF = objFCFs.Add(x:=0.125, y:=0.1, z:=0)
    objFCF.PrimaryFrame = "FLVB0.001MCVBA"
    'Add few vertices to the FeatureControlFrame
    Call objFCF.AddVertex(x:=0.2, y:=0.2, z:=0)
    Call objFCF.AddVertex(0.25, 0.225, 0)
    objFCF.BreakLine = True
    Call objFCF.GetVertices(VertexCount:=lngVertexCount, Vertices:=dblVertices)
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
    Set objFCF = Nothing
End Sub
See Also

FeatureControlFrame Object  | FeatureControlFrame Members