Solid Edge FrameworkSupport Type Library
SecondaryFrame Property
Description
Sets and returns the secondary frame text for the referenced FeatureControlFrame object.
Property type
Read-write property
Syntax
Visual Basic
Public Property SecondaryFrame As String
Example
Private Sub Form_Load()
    Dim objApp As SolidEdgeFrameWork.Application
    Dim objDoc As SolidEdgeDraft.DraftDocument
    Dim objSheet As SolidEdgeDraft.Sheet
    Dim objFCFs As SolidEdgeFrameworkSupport.FeatureControlFrames
    Dim objFCF As SolidEdgeFrameworkSupport.FeatureControlFrame
    ' Local variables to be declared here
    Dim strSecondaryFrame As String
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
        Set objDoc = objApp.Documents.Add("SolidEdge.DraftDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    On Error GoTo 0
    'Get the Active Sheet object
    Set objSheet = objDoc.ActiveSheet
    'Get the FeatureControlFrames collection object
    Set objFCFs = objSheet.FeatureControlFrames
    'Add a new FeatureControlFrame
    Set objFCF = objFCFs.Add(x:=0.1, y:=0.1, z:=0)
    Call objFCF.AddVertex(x:=0.3, y:=0.25, z:=0)
    objFCF.PrimaryFrame = "FLVB0.001MCVBA"
    objFCF.BreakLine = True
    'Set the data for SecondaryFrmae
    objFCF.SecondaryFrame = "SRVB0.003SCVBB"
    'Retrieve the data from SecondaryFrmae
    strSecondaryFrame = objFCF.SecondaryFrame
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objSheet = Nothing
    Set objFCFs = Nothing
    Set objFCF = Nothing
End Sub
See Also

FeatureControlFrame Object  | FeatureControlFrame Members